This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMH6321: How the output depends on the frequency (Sallen Key)?

Genius 17625 points
Part Number: LMH6321
Other Parts Discussed in Thread: TINA-TI

Hi Experts,

Seeking your assistance on this query:

Customer uses the TI filter design tool; there it selected the LMH6321. Where in the datasheet we can see which maximum output voltage will have at a 1 MHz signal?

They are designing an anti-aliasing filter with a cut off frequency at 1 Mhz (Sallen Key), and input signals are between -10 V and + 10 V. Therefore, it's important for them that the output voltage will be approximately +-10V too.

Thank you.

Regards,
Archie A.