Hi expert,
Customer measured t(low) = 1.23us in fast mode which is lower than DS minimum spec requirement 1.3us but no any communication issue.
Is it acceptable or any concerns?
Regards,
Allan
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Allan,
The spec is kept consistent with the protocol standard. The device actually has a more relaxed requirement. As is, the timing should be no issue.
Regards, Guang
Hi Guang,
One more question that the measured Vbase is 0.26V but 0V. Any concern about it?
Regards,
Allan
Hi Allan,
Since allowed logic-low level is 0.4V or below, 0.26V is within required range and is acceptable.
Regards, Guang