Part Number: LF353-N
Other Parts Discussed in Thread: LF353
hi,
what is the recommended operation Vcc range? From Figure.5 in datasheet, does it mean that the VCC range +-5Vmin----+-18Vmax?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Ken,
this figure only shows the tyical performance of LF353. This figure does not guarantee that the OPAmp works down to +/-5V and below.
On page 11 the datasheet says:
"Each amplifier is individually biased by a zener reference which allows normal circuit operation on ±6V power supplies. Supply voltages less than these may result in lower gain bandwidth and slew rate."
And footnote (3) on page 4 says:
"Supply voltage rejection ratio is measured for both supply magnitudes increasing or decreasing simultaneously in accordance with
common practice. VS = ±6V to ±15V."
So, I would say the recommended supply voltage range is +/-6V to +/-15V.
Kai