Part Number: LM321
Other Parts Discussed in Thread: TLV9301, LM7705
I'm using the MFX version with a 12V power supply to make a 0-10V signal. It works very well with a high-impedance load, but sometimes I need to drive a load with as little as 500 ohms. Is there a different part that I should be using? I really want to be able to drive with a single-ended power supply and go from 0 to 10V.