Other Parts Discussed in Thread: INA129, LMP7704, LMP2012QML-SP
Hello,
What is the thermal tail settling behavior of LMP7704-SP?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
What is the thermal tail settling behavior of LMP7704-SP?
Thanks
Ekam,
The response for this device is the same as what I gave you for the INA129. Let me know if you have additional questions:
Best regards,
Art Kay
Typically, we only show output setting in response to a step input voltage (see below for LMP7704) including settling time to 0.1%, 0.01% and sometimes 0.0015% (16 bits) - missing here as Kai pointed out..

As far as the thermal tail settling behavior goes, this would require characterization involving multi-dimensional matrix of change in the output voltage and/or load (power dissipation) for each type of package with different thermal resistance characteristics and for this reason it is seldom done. The best thermal settling time behavior would be obtained by using one of our zero-drift parts like LMP2012QML-SP (dual).