Other Parts Discussed in Thread: OPA350, OPA353, TLV4110
Hi,
I'm looking for an op amp, which is internally compensated, to be stable when drawing capacitive load of 10uF. The op amp has to be able to provide an output current of 100mA.
My supply voltage is limited to 5V. While searching in TI library, I could not find any parameter kind of "unity gain stability" or so to set... I came across OPA350 which can come along with cap loads, but its maximum Iout is 40mA.... Actually I will be using the op amp with an amplification factor of 2, so it doesn't really have to be unity-gain stable, but at least two-gain stable :)
Thx