This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMH6553: Is the slew rate definition differential or single ended?

Part Number: LMH6553


Hi!

The data sheet specifies the slew rate (at 4V Step, AV = 1) with 2300 V/μs. Is this value to be interpreted differentially, i.e. do the positive and the negative output pin reach "only" 1150 V/µs each?

Best Regards,

Andre