Part Number: TLV3502
Other Parts Discussed in Thread: TLV3501, TLV3604
TLV3502 seems to have very low input bias and offset current in pA at low propogation delay at 4.5ns.I presume that the input pin is connected to CMOS. LT1720 from linear technology with similiar config has 2uA bias current and price is also higher than TLV3502. I couldn't see many change in performance parameters except supply voltage which is little bit more than TLV.Since for my application I need very low bias current,I chose this comparator. My application requires TLV3502 to work as fast as 50ns since my input resets every 50ns.Can it work under such conditions?.Moreover, does TI provide any comparator with LVDS output at 1-5ns switch time and minimum bias current in pA-nA than in uA.