Other Parts Discussed in Thread: INA4180
Hi,
I am using the INA4180A1 current sense amplifier from which one of the 4 channels is unused. The device is implemented using a single supply rail.
I was wondering how to properly terminate it and I found the following article from TI: SBOA204A – October 2017. Figure 2 (right) illustrate a proper implementation of unused opamps using a single supply rail. However, in that case it is only applied purely on the opamp itself, whereas the INA4180 mounts internal resistors in a differential arrangement for obvious reasons.
In that sense, and in order to follow the approach of the aforementioned article, I thought about the following solution:

The addition of 475 kOhm resistors would make the series combination with Rint to be 500kOhm, so the gain factor would be unity, but also to have V+/2 at the positive input of the operational amplifier. Would that be an acceptable way to terminate it?
Many thanks in advance.
Best regards,
Pascual