Other Parts Discussed in Thread: TLV3801
Hi,
I am connecting the TLV3605 to a negative voltage (For example -1.7V) at its VEE pin. I know that the LVDS output will refer to the VEE pin as its ground reference, in this case, connecting a -1.7V to the VEE pin, the common mode voltage will become -0.5V.
However, I am DC biasing the output common-mode of TLV3605 back to +1.25V as below.

The comparator input will go up to 200MHz. I would like to know that with this practice,
1) In long term, will this degrade the comparator?
2) Will this cause long term reliability issue?
Thanks.