Hi guys,
I want to compare a PWM from [0-5V] to a voltage reference of 2V. I want the output of the comparator to be offseted to the following voltage [5-12]V so I' planning on putting the Vss pin to 5V and the Vdd pin to +12V. That way, a low level would give me 5V and a high level would give me 12V.
Can you confirm that I could use the LM2903BQDRQ1 with two different voltage supplies and no ground please?