to whom it may concern
We apologize for the sudden contact. My name is Daisuke Suzuki from Olympus DEM Technology 2.
Please tell me about the LMH6553 (differential amplifier).
・Regarding the output signal, is it prohibited to use Pch open and Nch 50Ω termination?
We would like to use this differential amplifier within our company, but on top of that, we would like to consider stopping the signal on only one channel.
Originally, I think that a single amplifier should be used, but it would be helpful if you could teach me.
(example)
Should the Nch side be open if the Pch side is open?
If the Pch side is 50Ω, should the Nch side also be 50Ω?
Is the Pch side open and only the Nch side 50Ω unusable?
Such an image.
Thank you very much.
=========================================================================
オリンパス株式会社
SES__Digital_Eng_and_Mfg__Electrical_Simulation_GLB__U1 鈴木 大輔
DEM技術2
daisuke.suzuki13@olympus.com
〒192-8507 東京都八王子市石川町2951
世界の人々の健康と安心、心の豊かさの実現
=========================================================================