This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3900: Need Application Note of my Configuration

Part Number: LM3900


Hi Team

I am debugging one of the board issue which has LM3900N. I could not understand the design configuration of below circuit. Could you please help to provide any application note for this?

Regards

Srikanth Kacchu

  • Hi Srikanth, 

    I could not understand the design configuration of below circuit.

    The op amp is configured as open loop without feedback, which it is using op amp as comparator in the application. In other words, the output will either go high or low, operated in saturation mode. In this case, Vout will be measured at 5Vdc or GND.

    The output results may be different if the circuit is operating in DC or Step/Transient events. 

    comparator 05092023.TSC

    The output of the top circuit is likely measured at GND, while the output of the bottom of the circuit will be measured at 5Vdc.   

    op amp vs comparators.pdf

    Please let me know if you have additional question. 

    Best,

    Raymond