Part Number: INA280
Hi Experts,
Good day.
We are trying to design a current sense circuit and we have a question about your Analog Current Sense amplifiers. Trying to measure the current flowing through a 1 Ohm resistor which is in series with a resistive load as well as a TEC. The circuit is being powered off of a +/-10V DAC output. I have +8V and -8V supplies to power a current sense amp from, but all datasheets show the amplifiers having a V+ and GND terminal. We really need the output to be bipolar because the circuit it feeds into is expecting a voltage in the range of +/-8V.
Question:
Can we use one of your current sense amplifiers like the INA280 and instead of using V+ and GND, use V+ and V- (+/-8V) as supplies? If not, are there any products that might suit our needs?
Regards,
Archie A.