Part Number: OPA855DSGEVM
Other Parts Discussed in Thread: OPA855, OPA859, OPA856, OPA861, TLV3603E
Hello E2E Experts,
Good day.
I am interested in powering a laser diode. It is a simple design, I have a clock generator that outputs +7dBm of power as a square wave. I want that to be amplified by the OPA855IDSGEVM at a frequency of 1 kHz. Then I want a series resistor at the output of the Op-amp to turn the voltage source into a current source that will be used to power the laser diode at 50mA. My question is if there is a way to add a series resistor to the output of the OPA855IDSGEVM on the board before reaching the SMA connector.
Id also like to know if +7dBm is enough to power as input into the OPA855IDSGEVM
And what the output power would be with +7dBm input so that I can calculate the series resistor I would need.
Regards,
CSC