Other Parts Discussed in Thread: TLV3801, , TLV3801-Q1
The following comparators (TLV3811, TLV3811-Q1 , TLV3801, TLV3801-Q1) have 3 imprecision into the datasheet
Power Supply
It's not clear whether Vee < 0 can be used when considering TLV3811. From Table 5-1, it appears that Vee can be a negative voltage, but nowhere are the minimum and maximum levels of Vcc and Vee reported. In Table 6.1, row 1, it seems that the difference between Vcc and Vee should respect a range (-0.3V; 5.5V), but not their absolute values. Is this correct? Can I have Vcc=2.5V and Vee=-2.5V, since Vcc-Vee = 5V?
Input Impedance
It appears from Figure 7.1 and paragraph 7.4.1 Input that the IN+ and IN- inputs are internally terminated at 50 Ohms. Is this correct? There is no table provided and Figure 7.1 does not show the complete circuit to understand it.
Random Jitter
How much is the random jitter of the device? no spec is present
Best
Nicola Lusardi