The INA126 is used the amplify the voltage difference from a strain gauge load cell. The circuit is in the attached picture. We are experiencing failures were it appears that the input stage of the INA126 is damaged. On the failed units the input resistance measures 70KOhms between pin 2 and pin 3 without any power applied. Do you see issues any with the design? Is there a better circuit topology that could used? Thanks.