Part Number: OPA548EVM
Other Parts Discussed in Thread: OPA548,
Hello!
I am trying to find out why my OPA board is not working as it should.
I am powering the dev board using a peaktech 6225A . I am using the -30V output from the power supply into the AVSS on the dev board. same for the ground.
I am using J2 to send in my signal from an function generator with a sine wave signal at 2VPP.
The output to the voice coil is not powerful enough to get it running. Is there a way I could debug the board and find out if there is something fried on the board or some connection might have been wrong in the pricess which lead to the OP amp to act weirdly, or is it the power supply I am using which is not sufficient enough? Please advise and thank you