Other Parts Discussed in Thread: TINA-TI
I need a VCA824 model with 14 pins, but when importing the Pspice model of the VCA824 into ADS, this model is not in the options,please tell me why?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Thank you for your question. With the 14-pin package, two pins are duplicates of the supply rails and one pin is a no-connect, meaning it is not used.
We typically do not have these repeated pins on the P-Spice or TINA-TI model because it does not impact the functionality of the model and would make the model more complicated without adding any benefit.
If you remove those duplicated or unused 3 pins, that would result in the 11-pin model.
Thank you,
Rachel