This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV6001: Back calculating the input from output signal chain with Isolated Amplifier and opamp

Part Number: TLV6001
Other Parts Discussed in Thread: AMC1350

Hi Team,

We are measuring the voltage of a charger using the below circuit with the help of an ADC present in a uC.

The value of charger voltage is required for some other applications.(he value of charger voltage is used to calculate isolation resistance).

So I tried to calculate the input from output. I am getting an error of almost 2V in my calculations.

We are using AMC1350 and TLV6001 in the signal chain.

Please see my circuit diagram and calculations below.

From the circuit diagram you can see that the input V2 is 58V.I used the equation shown in the second image to calculate V2 from Vout.

I am getting a value of 56V instead of 58V.May I know where I went wrong.