Part Number: LMP8350
Other Parts Discussed in Thread: TINA-TI
Hello
thank you for your reply.
I have an additional question.
If the Vocm voltage is supplied externally, what is the current consumption of Vocm?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
The total amount of sinking/sourcing current from an external reference voltage will depend on you external circuitry and your output common-mode voltage requirements. The device datasheet shows the internal circuitry of the Vocm pin of the device, and suggests buffering (low-impedance output) your external voltage divider + voltage reference.
The external current needed to sink/source to the internal circuitry can be calculated using the below equation: (replace 50kOhm with 60kOhm)

Below is an example when setting Vocm to 1.5V with single supply of 5V:

The Tina-TI simulation file is attached below.
Thank you,
Sima