Part Number: TL082
Hi team,
My customer would like to use TL082 in a differential proportional circuit. Is there a risk of loop instability if the amplification gain is less than 1, such as input is 10V, output is 1V?
Thanks in advance.
Regards,
Ivy
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Ivy,
It is not the signal gain that matters. It is the amplifier's noise gain which is the closed loop gain as viewed from the IN+ pin (when feedback is passed to IN-) .
Stability becomes a concern when extra gain or delay is added to the loop.