Part Number: INA239
Other Parts Discussed in Thread: ISO7763, ISO7741, INA238
Hi!
I need help with using a low side sensing application with the INA239.
So far I have it working with a high-side sensing application but it does not work for the low side sensing application. Also I would like to add that it only works when I share the common ground of the two PSU's (power supplies). Please refer to my wiring diagram that illustrates the + and - wires of my system.

I tested the low-side sensing by moving the shunt resistor from the positive leg to the negative leg and adjusted the two wires that goes to the INA239 accordingly but I got no readings. I then checked the voltage on the negative side and realized there is no voltage on the negative leg therefore I get no readings.
May someone assist me with the wiring diagram of for the low-side sensing?
Thank you