Other Parts Discussed in Thread: OPA2189, OPA2994
Hi team,
we want to do p2p upgrade on LM6142BIMX/NOPB on customer side. Could you please kindly help provide comparison table between LM6142/ OPA2994/OPA2189 ? Thanks.
BRs
Given
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hey Given,
| ► Part Number | LM6142 | OPA2994 | OPA2189 |
| Manufacturer | TI | TI(Pre-production) | TI |
| Channel Count | 2 | 2 | 2 |
| Vs Range | 1.8V to 24V | 2.7V to 32V | 4.5V to 36V |
| GBW (MHz) | 17 | 25 | 14 |
| Slew Rate (V/µs) | 25 | 18 | 20 |
| Vos max @ 25oC (mV) | 1 | 1.5 | 0.005 |
| Vos Drift, typ (µV/oC) | 3000000 | 1 | 6000 |
| Rail-to-Rail | In, Out | In, Out | In to V-, Out |
| IQ typ (mA) | 0.65 | 1.1 | 1.3 |
| Vn at 1kHz (nV/√Hz) | 16 | 12 | 5.2 |
| ISC typ (mA) | 8 | 150 | 65 |
| IBias (typ) (pA) | 180000 | 100000 | 70 |
| Operating Temperature (°C) | -40 to 85 | -40 to 125 | -40 to 125 |
| Available Packages | PDIP-8, SOIC-8 | SOIC-8, VSSOP-8, SOT-23-THIN-8*, WSON-8*, X2QFN-10* | SOIC-8, VSSOP-8 |
Here is the comparison table. I am also sending you an email on how you may generate these tables without the need to wait for an E2E response.
Best,
Jerry