Other Parts Discussed in Thread: LM393LV
Hi team,
Could you please kindly help provide comparison table between LMV393IDR and LMV393LVDR ? Thanks.
BRs
Given
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Given,
I believe you meant the LM393LVDR.
| ► Part Number | LMV393IDR | LM393LVDR |
| Manufacturer | TI | TI |
| Pinout | Dual | Dual |
| Channel Count | 2 | 2 |
| Package | SOIC-8 | SOIC-8 |
| Package (TI Equiv) | D8 | D8 |
| Vs min (V) | 2.7 | 1.65 |
| Vs max (V) | 5.5 | 5.5 |
| Response Time, typ (µs) | 0.28 | 0.6 |
| Vos max 25°C (mV) | 7 | 2 |
| Input Range | To V- | R-R |
| Output Type | OC | OC |
| IQ (max) (mA) | 0.15 | 0.035 |
| IBias (typ) (nA) | 25 | 0.005 |
| Temperature Min | -40 | -40 |
| Temperature Max | 125 | 125 |
| Additional Features | POR, FailSafe, Vout>V+ | |
| Auto Qual | ||
| GPN | LMV393 | LM393LV |
| Datasheet | LMV393 | LM393LV |
| TI Web Page | LMV393 | LM393LV |