Part Number: LMP2022
I am using the LMP2022 in a buffer configuration for triangle wave signals that have an offset. The amps in the design are powered with a single sided 5V supply. The signals are above the closed loop bandwidth recommendation of 20kHz (to avoid aliasing from the auto zero circuit). However, the datasheet also says that signals above 20kHz are not affected.
What is the max Vout-pk for signals at 600kHz? What about for 300kHz?
Thanks,
Nicole