Other Parts Discussed in Thread: OPA356
I have OPA2810 and OPA356.
I'd like to configure OPA356 as I-V converter(Photodiode)
and OPA2810 as second non invert or invert amplifier(integrator, G=10)
AFAIK, some OP-AMPs supplied with asymmetric power rail, then would get a bias = (V+ - V-)/2 + v-
For instance,
I supplied some OP-AMP with +4.5V and -2.5V, and input is 0V, configure this OP-AMP as follower buffer.
I would get output bias: (4.5 - (-2.5))/2 + (-2.5V) = 3.5V + (-2.5V) = 1V
Has OPA2810 and OPA356 a problem?