Part Number: AMC1311
Other Parts Discussed in Thread: AMC3330, AMC1350
Hello.
As title, I looking for isolated amplifier product that can perform differential input and differential output function.
A product that matches Output type(differential), range(2 Vpk-pk) and gain(1) is AMC1311, but it is single-ended input type.
So, I ask if it is possible to operate by implementing differential input(2 Vpk-pk, actually -1~1 V) without connecting the input to GND in the product.
Apart from the above, It would be convenient to have the filter below.(This is a suggestion based on my personal opinion.)
At 'Isolated amplifiers' - gain, bandwitdth, input type, output type.
At 'Precision ADCs' - PGA (Y/N, Min,/Max.), variable gain(Y/N, except PGA), variable offset(Y/N), selectable input range list
At 'Precision DACs (≤10 MSPS)' - output type(single-ended/differential), variable gain(Y/N), variable offset(Y/N), selectable output range list
Thank you.