Other Parts Discussed in Thread: INA331, TINA-TI, LM27762, AFE5816, OPA325
Hi
I'm implementing below circuitry for amplifier section. The input signal voltage will range between 10uV to 10mV. But in the current circuit, the offset is set by feedback circuit which i observe as not working. When a 1 mV signal is given with less than 3mV offset, output is getting clipped. Vref pin is not connected to any external voltage.

I would like to connect the external voltage to increase input offset such that a gain between 100-200 can be set for the input 1mV signal. Suggest modification to be done for the same. Will giving Vref voltage result in amplification of that offset voltage also.
Can i set offset by connecting capcitor to ground for Vref pin, if so what should be minimum value of capacitor.











0