Part Number: ISO224
I am not getting proper ouput sinusoidal swing also the ouput is not shifted by 2.4V as mentioned in the datasheet.
Vin=3V,sinusoidal


This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ISO224
I am not getting proper ouput sinusoidal swing also the ouput is not shifted by 2.4V as mentioned in the datasheet.
Vin=3V,sinusoidal


Hi Apoorva,
The output of the ISO224 will be +/-4V differential with a full-scale input voltage, or +/-1/3*Vin.
As the INA is connected, with a single-supply and GND setting the common-mode at the inputs, the INA cannot drive below ground.
Please see this document for an example of a correct circuit: https://www.ti.com/lit/an/sbaa317/sbaa317.pdf
Hello Alexander,
I want to verify for the individual performance of IC ISO224, so if I took out the INA224, now if I check with Individual pins with respect to the ground I am getting the proper output as per the datasheet, but with respect to the differential pins, I am not getting the proper values. can you please tell me how to simulate it in the proper way.
Regards,
Apoorva


Hi Apoorva,
The outputs are driven and they are shorted to ground in the design. The device would be damaged if operated in this way. Add a resistor between the output and ground in order to limit the current.