This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA216: INA216A2 PSpice Model (Rev. B) can't work in Micro-Cap

Part Number: INA216

Hi TI expert:

I am using Micro_Cap 12.2.0.5 to do the simulation, I used Part Winzid loading INA216A2 PSpice Model (Rev. B) to MC12 lib. ​But I can't find the proper Shape for INA216 as INA216 is 4 pin device and an ordinary OPAMP is a 5pin which has a separate Vdd pin.

When I run the simulation, it appears error information:

----------------------------------------------------------------------------------

Error: Node INM from subckt INA216A3 does not match any defined pin name for this part.

This error occurs when a pin name (or number) from the subcircuit statement doesn't match any of the pin names in its Component library definition.
To fix the problem, make sure that each of the pin names listed in the .SUBCKT statement in the subcircuit file corresponds to one of the pin names listed in the Component library.

---------------------------------------------------------

Would TI expert pls. advise the proper MC-12 Shape for me?

Thanks