HEllo
i developped a new product with the PGA309 and i have problems when i program it with Pins TEST,SDA,SCL and GND ( TWo Wire access)
Sometimes , the pga309 breaks ( Logic circuitry) and i am looking for the cause/reason
It is possible that i apply a level '1' to the pin TEST when the PGA309 is not supplied
Do you know this problem ?
Do you have the input circuit of the PIN TEST ?
Do you Have other ideas that could cause this destruction?
Thanks you for your answers
FREDERIC