Other Parts Discussed in Thread: OP07, TL331, TL331B, TLV1861, TLV3011B, TLV3401, TLV7011, LM339, LM393
Hi,
I want to use an OP-amp (OPA2202) in comparator mode to compare the voltage of a lithium battery with a fixed voltage. As the circuit always is not ON, I need to know how much the input pin of the OP-AMP consume current in not only in off sate of the OP-AMP but also in ON state of that because if it is too much the battery quickly will be drained.
I have attached a schematic of the circuit.
Regards,
Saeed