Other Parts Discussed in Thread: TLV3501
Hi
while using this chip in one of our boards, we notice that the SHDN does not function as excepted. in order to be sure we designed a simple test board:

in this design pin 1 (IN-) connected to 3.3V via 10K resistor, pin 3 (IN+) connected to GND, pin 4 (VCC = 3.3V).
pin 6 (SHDN) is connected to a micro-processor. this signal is toggled in a very low frequency. each time that the SHDN go's from HI to LO we see a pulse in the output (pin 5) although the 2 input pins are connected to DC:
Yellow: SHDN
Blue: output

do you have any explanation for this behavior?
how it can be avoided?
attach the two fogures.
Thanks 
Alon Shemesh