Part Number: THS6182
Hello,
I'm using 2 THS6182 as a power amplifier to amplify sine wave in 220KHz,
while testing the circuit I found a DC offset of 2V yet my inputs are AC coupled and measured and didn't have any DC offset between them.
my load is from 10ohm to 250ohm,and i found the offset with load and with high impedance load.
Iadj pin is tied to the ground.
Attached is my circuit :

and the output measured on FB303 (capacitor side):
any idea how to avoid the offset?