Part Number: OPA2392
Dear Team,
please tell me at which chopper frequency OPA2392 works.
Kind regards
Bernd Hafen
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: OPA2392
Dear Team,
please tell me at which chopper frequency OPA2392 works.
Kind regards
Bernd Hafen
HI Bernd,
The OPA2392 is a high precision, low -offset linear amplifier. It offers very low offset ±10 µV (maximum) and low-drift: ±0.18 µV/°C.
However, this amplifier uses e-trim technology to achieve the high-precision; therefore it is not a chopper, and there is no chopper frequency associated.

Attached is an application note describing the different circuit techniques used to minimize offset in amplifiers that may be of interest:
Thank you and Kind Regards,
Luis