Other Parts Discussed in Thread: OPA387, OPA392, OPA182, OPA192
TI App Note SLOA059B "DC Parameters: Input Offset Voltage (VOS)" (Richard Palmer and Katherine Li), talks about op-amp input offset voltage but may not contain an answer to the following:
I'm designing a circuit that uses a quad op-amp IC. I'm specifying a very low input offset voltage device (Vos) so the circuit can meet specifications. However, if the Vos of all 4 devices on the chip matched (or came close) and tracked each other, that would be sufficient.
My question: In a single-die multi-opamp package, are the offset voltages matched? If not, are there devices which are better designed for matching than others?
My guess: Automated Vos trimming probably disturbs what would otherwise be a perfect match.