Looking for data at Vcc = + 15 V, V_o(pp) = 20V or greater, with Gain = 3, 5, and 10. Or the closest data available.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Looking for data at Vcc = + 15 V, V_o(pp) = 20V or greater, with Gain = 3, 5, and 10. Or the closest data available.
Hi Donald,
Unfortunately, I did not find additional data for this device, therefore all the relevant data for the THS3491 that was collected is highlighted in the datasheet. We do have models for these devices if you would like to simulate different configurations you are interested in. We also have EVMs for these devices, which we suggest as well for more assuring data compared to simulations.
Best regards,
Ignacio