Part Number: OPA189
Dear TI team
I have a question related to the content of the thread below.
Since the supply voltage of the amplifier in front of the OPA189 is ±10V, -5.5V, which exceeds the absolute maximum rating, may be momentarily applied to the -input via a 1kΩ resistor.
So I have the following two questions.
(1)There is a clamp diode at the input of the OPA189. What is the Vf of this diode?
(If the Vf of this diode is sufficiently high, I believe that the absolute maximum rating can be avoided. I was able to confirm through simulation that the absolute maximum rating is not exceeded.)
(2) Please let me know if there are any points to note when adding an external 5V clamp circuit to the front stage of R1 (1kΩ) in the attached circuit.
Best Regards,
Taroimo