Other Parts Discussed in Thread: OPA549, OPA567, OPA569
Good day everyone,
I need to design a current amplifier circuit that drives approximately 220 mH coil, 2 Ohm series resistance with an alternating current of 25-50 kHz, 5V amplitude and a current of approx 1A.
I have referred to this forum for some research, and some users suggested using an "Improved Howland Current Pump" (IHCP). Someone even provided its design design principles as shown in the following link.
I have followed those steps, and have managed to develop a current source in the mA range. However, when I try to increase the frequency or inductance, the output current and voltage waveforms become distorted. I have included my TINA TI simulation files.
What are the design steps that I can follow to optimize this circuit for:
- Higher inductance ~220 mH
- Higher frequency 25-50 kHz
- Higher output current ~1A