Part Number: OPA860
Hi Kailyn & Kai,
I am practicing with the OPA860 peak detection circuit that Kailyn post.
e2e.ti.com/.../opa860-opa860-sample-hold-circuit
The circuit is consist of two-stage of OPA860. The first for a fast rise time and the second for a slow decay time.
The circuit can sample a pulse width of 1ns. It is really impressive.
I am wondering what will happen if the input instead of continuous sine wave.
I know that will output a very low frequency signal, even looks like a DC signal.
Below is my schematic, I used various frequency of sine, the same amplitude.
Why the output of DC voltage will drop when the frequency rise? Is it a bandwidth limitation?




Thanks so much.
SK.