Part Number: TLV9022
I am struggling to create a latch out of this. As this one doesn't have inbuilt hysteresis, I have chosen the resistor values and when current is 5.5amps, i.e around 0.11 volts with my 200mOhm resistor, I want the output to go high -> turn the P-Channel Mosfet OFF and disconnect the load from the power supply. I was able to do the hysteresis part, but I am struggling to make it work with the MOSFET. Any help on this would help me complete my project.
If i remove the MOSFET, i get the latching, but not with it, nothing seems to work with the mosfet attached