Part Number: INA241A
Other Parts Discussed in Thread: LM324
Hi Team,
My customer is using INA241A5 with 200V/V gain and a 0.4mohm shunt current to sampling the maximum 50A current. The supply of VSS and GND is 12V and -7V for sensing the bidirectional current.
To maintain the high CMRR, they add capacitors on IN+ and IN-, because they observed that when the common mode voltage changes from 3V to 2.9V there is a 100mA error of INA241. So they add a 4.7uF capacitor on IN- and IN+. However, the problem of the response time then exists. When there is a 50A through the shunt for 2ms, the output voltage is quite unstable. It seems stable when the time raise to 10ms (50A lasts for 10ms). The output signal can be read as a stable signal. Based on the trade off between the CMRR and response/settle time, customers have some questions:
1. Are there any methods to achieve the better CMRR and the faster settle time ? Currently it seems customers cannot find a good way to balance this, hope that you can give some advices.
2. For the 12V and -7V supply for INA241, could this asymmetric supply voltage be a problem?
Pls give some suggestion on this, thanks!
Manu