Part Number: INA592
Other Parts Discussed in Thread: DAC80502,
Hello Team,
We are designing with INA592IDT for a Howland current source as per the technical documentation Analysis of Improved Howland Current Pump Configurations.
Attached is the circuit for the same.
The signal DAC_CH_A is from a DAC (DAC80502DRXT) and the voltage varies from 0V to 5V.
The current thus generated is used as the excitation current of some RTD sensors like PT100, PT1000, and diode.
We are currently developing the firmware with a decade box as the load resistor (Sensor).
As the resistance is changed from 1K to 3K gradually, the current seems to be increasing (the current is initially set to 1mA, using the DAC voltage and resistance using mux).
When we measure the voltage at the DAC, the DAC voltage seems to be stable at the voltage we set for 1 mA.
But the voltage at the resistor R150 (node between R150 and C127), the voltage seems to be increasing as we increase the load resistance using the decade box.
What can be the reason for this?