HI all:请教一个问题:我图片2里面这个用INA241A5-Q1搭建的电路的Vout,是按照图片1里这个公式计算吗?还是直接Vout= I× RSENSE × G就可以,谢谢1.zip
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI all:请教一个问题:我图片2里面这个用INA241A5-Q1搭建的电路的Vout,是按照图片1里这个公式计算吗?还是直接Vout= I× RSENSE × G就可以,谢谢1.zip
Hi,
是按照图片1里这个公式计算
Regards, Guang
Hi luo sui,
REF1/REF2接地,可以按照Vout= I× RSENSE × G来计算Vout. This configuration provides maximum dynamic range for a unidirectional current measurement application.
Even though the output won’t surpass the supply which is 3.3V, and the ADC won’t see more than 3.3V, it is a good idea not to clip the output signal.
Regards, Guang
HI Guang:
it is a good idea not to clip the output signal.
请问意思是不要对Vout再用分压电阻进行分压,然后再输出给MCU吗?
另外,有没有INA241A5-Q1的替代料可以推荐,谢谢
Hi luo sui,
By “not to clip the output signal”, I meant to say that the maximum output voltage (Vout= I× RSENSE × G) should be smaller than the power supply 3.3V.
For INA241A5-Q1的替代料 – we have a large selection of current sense amplifiers, you can browse from this link. You’d have to define how similar the replacement is to INA241.
Regards, Guang