I'm using INA321 for high side current measurement of MSP430, and I have the following questions:
1) In the data sheet, it is not mentioned, which is the minimal differential shunt voltage that can be measured by INA321. Does this change with common mode voltage?
2) I set the shunt=100 Ohm, and I sweeped the current from 0A ... 100uA. I got the following results (attached). In the data sheet it is not mentioned that the gain changes with the load current. How could you explain this? The plot shows that the gain gets stable at the end, but this is not really true, because for ex for 100uA, the gain is 92,22 and for 50uA it is 88,85.