Other Parts Discussed in Thread: INA240
Hi, TI support team
Inquiries about the current sensor to be applied to the concept below have been received from the customer.
Application: Low-frequency massage device
Detail : A product that delivers low-frequency stimulation with two pads connected to the device
The solution the customer is looking for: A sensing solution to stop the operation of the device when one or both of the two PADs fall off the skin.
The customer wants to know if sensing is possible through the current sensor (INA240).
I am attaching the block below.

It is a structure that outputs the frequency by loading it on the PWM.
Since the device has to stop operating even when one pad is dropped, sensing for each line of Ch1 and Ch2 shown in the block below seems necessary.
The reason (see waveforms below) is that the waveforms for 1 PAD drop and for all drop cases are the same as 1-2.
I share the waveform received from the customer.
This is the waveform when only PWM is output and when Frequency is output together.
1. PAD CH1, CH2 output: MAX Level + Frequency
1-1. [Max Level unplug PAD]
1-2. [Max Level plug PAD]
2. PWM output : MAX Level
2-1. [Max Level unplug PAD]
2-2. [Max Level plug PAD]
If there are other sensing methods applicable to this solution, please recommend them.
Can I use TI's current sensor (INA series, etc.) to sense the power signal such as the attached waveform?
Please let us know if you have additional questions.
I will answer you.
Thanks.
Regards,
MJ