Part Number: LMP7731
Hi,
The below graph of the input bias current of LMP7731, I want to make sure I understand what direction these currents have.
Is it per default considered the current direction is into the (+) and (-) terminals?

Thank you
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LMP7731
Hi,
The below graph of the input bias current of LMP7731, I want to make sure I understand what direction these currents have.
Is it per default considered the current direction is into the (+) and (-) terminals?

Thank you
Thank you fore the very quick answer.
Just as a follow question, these current sources in I_BIAS CANCELLATION CIRCUIT, they are supplying bias for the NPN transistor pair, when the inputs are far from the supply rails. But if the input voltage is high then it is not enough and current starts to flow into the IN+ and IN- terminals?
Correct. (When the input is too high, the current source does not work, and all the base current must flow through the input pin.)
Adding my two cents, since the input bias cancellation scheme is not exact, and may over or under compensate the actual base current required by NPN input transistors, the actual direction of the current within the LMP7731 linear input voltage range may of either polarity, which is shown below.

Hi,
OK thank you for the input, that maske sense to me.
In my application, I could see that when my inputs came close to the positive rail, more current started to flow input the inputs and I got some offsets.
But it all makes sense now.
Thank you both the support.