This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV4051: Power-up state of output when input between Vit+ and Vit-

Part Number: TLV4051


When the LTV4051R2 comes out of power-on-reset and the input is between Vit+ and Vit- (ie, between 0.176V and 0.204V) is the output low or high? Unless I missed it this is not indicated in the datasheet.

Thank you,

Ben