This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TL103W: RC Calculation

Part Number: TL103W
Other Parts Discussed in Thread: UCC256403

Hi,

How to calculate the R and C values which are connected to pin 1 (Output) and Pin 2 (Inverting Input) and same as the Pin 7 (output) and Pin 6 (inverting Input. We have designed the CC CV charger 14.6V 30A using UCC256403. But we are facing a problem in CC mode. We used the TL103W as a CC/CV controller. CV is working fine but CC is working only the battery is connected after Power ON the charger. If we connected the battery before power ON the charger means, we are getting problem in CC mode. At that time Current comes to 5 to 6A instead of 30A. So please let me know how to calculate the R and C values. Is that R and C are the time constants of the correction?

Kind Regards,

Nishanth M